Data Fields |
|
struct { |
| uint32_t WindowCount |
| uint32_t TimeOutCount |
| uint32_t CR |
| } | W |
|
struct { |
| uint32_t WindowCount |
| uint32_t TimeOutCount |
| uint32_t Reserved2: 23 |
| uint32_t RandomKeyModeEn: 1 |
| uint32_t ResetWhenInvalid: 1 |
| uint32_t WindowModeEn: 1 |
| uint32_t GenerateIsr: 1 |
| uint32_t HardLockEn: 1 |
| uint32_t SoftLockEn: 1 |
| uint32_t Reserved: 1 |
| uint32_t StopEn: 1 |
| uint32_t DebugEn: 1 |
| uint32_t Enable: 1 |
| } | P |
The documentation for this union was generated from the following file: